OS Upgrade

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,102件の閲覧回数
stp1200
Contributor I
If we upgrade our operating system from Windows 2000 to Windows XP, can we use the same license file when we reinstall Codewarrior on XP?

I'm using Codewarrior 3.1 for the HCS12, single user license (no usb dongle).

Thanks,
-shane
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,585件の閲覧回数
BlackNight
NXP Employee
NXP Employee
Hello,
yes, Codewarrior licenses are independent from the Windows version (XP, XP home, 2000, etc).

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,586件の閲覧回数
BlackNight
NXP Employee
NXP Employee
Hello,
yes, Codewarrior licenses are independent from the Windows version (XP, XP home, 2000, etc).

Erich
0 件の賞賛
返信