No source available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No source available

1,892件の閲覧回数
konstantinoshal
Contributor I

Hello,

 

We are developing a project using MC9S08AC96 and CW 10.5 in assembly language.

The code is using banked memory. The problem is that when we put a

breakpoint in banked memory or stepping into , the debbuger is halted and displays the

message:

 

no source available for "0x0098A9 (0x0098A9)()"

 

If we don't use breakpoints the debugger is running without problems.

 

The same project is running fine in the old CW 6.3 - with and without breakpoints.

 

Can anybody help?

 

Thanks in advance.

 

Konstantinos.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,723件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

please test if remove .metadata folder under workspace then restart CW can solve the problem.

if not, please upload your project. this needs to be tested.

0 件の賞賛
返信

1,723件の閲覧回数
konstantinoshal
Contributor I

Unfortunately removing the .metadata folder did not solve the problem.

I can't upload the original project as it is used in a commercial product, but i have

attached a small project which demonstrates the same problem.

0 件の賞賛
返信

1,723件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

is your problem solved now?

0 件の賞賛
返信