No source available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No source available

1,983 Views
konstantinoshal
Contributor I

Hello,

 

We are developing a project using MC9S08AC96 and CW 10.5 in assembly language.

The code is using banked memory. The problem is that when we put a

breakpoint in banked memory or stepping into , the debbuger is halted and displays the

message:

 

no source available for "0x0098A9 (0x0098A9)()"

 

If we don't use breakpoints the debugger is running without problems.

 

The same project is running fine in the old CW 6.3 - with and without breakpoints.

 

Can anybody help?

 

Thanks in advance.

 

Konstantinos.

Labels (1)
0 Kudos
Reply
3 Replies

1,814 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

please test if remove .metadata folder under workspace then restart CW can solve the problem.

if not, please upload your project. this needs to be tested.

0 Kudos
Reply

1,814 Views
konstantinoshal
Contributor I

Unfortunately removing the .metadata folder did not solve the problem.

I can't upload the original project as it is used in a commercial product, but i have

attached a small project which demonstrates the same problem.

0 Kudos
Reply

1,814 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

is your problem solved now?

0 Kudos
Reply