NE64 bootloader code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NE64 bootloader code

跳至解决方案
2,528 次查看
eddie
Contributor I
I find that I need to implement a serial
based flash bootloader for the MC9S12NE64
using CW4.5.This looks a little difficult to
implement.Is sourcecode available for this sort
of application?
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,799 次查看
mjbcswitzerland
Specialist V
Eddie

The Freescale serial monitor is a good starting point - maybe it will do all that you require (?).

See the following for software and an application note on how to load it to an NE64 with a build-it-yourself BDM (using the NE64 DEMO board):

http://www.utasker.com/docs/documentation.html (under projects and application notes).

Regards

Mark Butcher

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,800 次查看
mjbcswitzerland
Specialist V
Eddie

The Freescale serial monitor is a good starting point - maybe it will do all that you require (?).

See the following for software and an application note on how to load it to an NE64 with a build-it-yourself BDM (using the NE64 DEMO board):

http://www.utasker.com/docs/documentation.html (under projects and application notes).

Regards

Mark Butcher
0 项奖励
回复