NE64 bootloader code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NE64 bootloader code

Jump to solution
2,527 Views
eddie
Contributor I
I find that I need to implement a serial
based flash bootloader for the MC9S12NE64
using CW4.5.This looks a little difficult to
implement.Is sourcecode available for this sort
of application?
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,798 Views
mjbcswitzerland
Specialist V
Eddie

The Freescale serial monitor is a good starting point - maybe it will do all that you require (?).

See the following for software and an application note on how to load it to an NE64 with a build-it-yourself BDM (using the NE64 DEMO board):

http://www.utasker.com/docs/documentation.html (under projects and application notes).

Regards

Mark Butcher

View solution in original post

0 Kudos
Reply
1 Reply
1,799 Views
mjbcswitzerland
Specialist V
Eddie

The Freescale serial monitor is a good starting point - maybe it will do all that you require (?).

See the following for software and an application note on how to load it to an NE64 with a build-it-yourself BDM (using the NE64 DEMO board):

http://www.utasker.com/docs/documentation.html (under projects and application notes).

Regards

Mark Butcher
0 Kudos
Reply