NE64 bootloader code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,498件の閲覧回数
eddie
Contributor I
I find that I need to implement a serial
based flash bootloader for the MC9S12NE64
using CW4.5.This looks a little difficult to
implement.Is sourcecode available for this sort
of application?
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,769件の閲覧回数
mjbcswitzerland
Specialist V
Eddie

The Freescale serial monitor is a good starting point - maybe it will do all that you require (?).

See the following for software and an application note on how to load it to an NE64 with a build-it-yourself BDM (using the NE64 DEMO board):

http://www.utasker.com/docs/documentation.html (under projects and application notes).

Regards

Mark Butcher

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,770件の閲覧回数
mjbcswitzerland
Specialist V
Eddie

The Freescale serial monitor is a good starting point - maybe it will do all that you require (?).

See the following for software and an application note on how to load it to an NE64 with a build-it-yourself BDM (using the NE64 DEMO board):

http://www.utasker.com/docs/documentation.html (under projects and application notes).

Regards

Mark Butcher
0 件の賞賛
返信