Microcontroller not supported by Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Microcontroller not supported by Processor Expert

跳至解决方案
4,087 次查看
Yuping
Contributor I

Hello All,

 

I am working with an MC68HC912B32 microcontroller.

I have simulated couple projects with CodeWarrior v5.1. 

Now I want to download the projects to the microcontroller. But when I was trying to do "Device Initialization", I got a message saying that MC68HC912B32 is not supported by Processor Expert.

Is there any way that can solve this problem?

 

Thanks!

 

Yuping

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,725 次查看
CrasyCat
Specialist III

Hello

 

No you can create a project for MC68HC912B32 using the wizard and you can debug on the target board using any

of the available connection (P&E Multilink, ...).

 

You will not be able to get ProcessorExpert to generate initialization code for the peripheral I/O.

For this microcontroller you will need to either search for sample code on the web of write your peripheral drivers yourself.

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,725 次查看
CrasyCat
Specialist III

Hello

 

No. Processor Expert and Device Initialization are only available for HCS12 and HCS12X microcontroller.

They cannot be used with older HC12 parts.

 

CrasyCat

0 项奖励
回复
3,725 次查看
Yuping
Contributor I

So you mean I can't connect the board I am using and download the program with CodeWarrior?

Thanks!

 

Yuping

0 项奖励
回复
3,726 次查看
CrasyCat
Specialist III

Hello

 

No you can create a project for MC68HC912B32 using the wizard and you can debug on the target board using any

of the available connection (P&E Multilink, ...).

 

You will not be able to get ProcessorExpert to generate initialization code for the peripheral I/O.

For this microcontroller you will need to either search for sample code on the web of write your peripheral drivers yourself.

 

CrasyCat

0 项奖励
回复
3,725 次查看
Yuping
Contributor I

Hi CrasyCat,

 

Thanks for your help!

I have a USB Multilink connector now. And I'm trying to do P&E Multilink simulation.

When I tried to debug the project, I got the error

FP: no programming voltage

I searched online and found somebody fixed it with providing the board with a 12v supply.

The board I am using is an M68EVB912B32. In the device overview here http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M68EVB912B32

it said +3 to +5-volt DC operation, so 12v supply is not safe for this board, right?

 

If so, what else could I do to fix this problem?

There is another thread https://community.freescale.com/thread/12974

But I don't understand the guy's explanation...

 

Thanks,

Yuping

0 项奖励
回复
3,725 次查看
kef
Specialist I

12VDC should be applied to Vpp connector and jumper W7 should be set to position 1-2. See user manual for this board