Manually installing service packs in CodeWarrior 10.x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Manually installing service packs in CodeWarrior 10.x

793 Views
dereksnell
NXP Employee
NXP Employee

With the Eclipse-based CodeWarrior 10.x, CW can be updated within the IDE using the on-line method.  This is a great way to see what updates and service packs for new devices are available.  There is a video link here showing the on-line update method.

 

The on-line method is preferred, but sometimes the manual method is required.  This could be for an update that is not yet released on the web, or not in the updater repository yet.  Or perhaps you are having issues using the on-line method.

 

If you need to use the manual method, you can find a list of updates to manually download and install here.

 

And here is a video link explaining the manual installation method.

 

 

 

Message was edited by: Derek Snell Fixed the video link

Labels (1)
0 Kudos
Reply
0 Replies