Making LIBS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Making LIBS

7,728件の閲覧回数
etolocka
Contributor I
Hi!

I´m using CW for HC(S)08 and I´m a little confused about the right procedure to make a LIB file from several ".c" files with functions.

Any advice?

regards,
Ernesto
http://www.desarrollos.tolocka.com.ar
http://www.mundomicro.com.ar
ラベル(1)
タグ(1)
0 件の賞賛
返信
6 返答(返信)

3,503件の閲覧回数
lucianon
Contributor I
Spoiler
 

this is my contribution to undestand how to make libs on CW6.

 

lib (it is the project to generate "out.lib")

testelib (it is the project that are using this generated lib "out.lib") 

 

Luciano Nicolau

www.tci.ind.br

 

0 件の賞賛
返信

3,503件の閲覧回数
lucianon
Contributor I

here are attached the projects to understand how to create libs on CW6.3 .

Luciano

0 件の賞賛
返信

3,503件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
to create a library, switch the Linker in the "Target Settings" page from "Linker for HC08" to "Libmaker for HC08". Then a new Libmaker for HC08 page shows up where you can specify the library name.
0 件の賞賛
返信

3,503件の閲覧回数
etolocka
Contributor I
Thank you!

Do I need to remove all libs and headers from the LIB folder in the Project Manager? (e.g. ansi.lib)

Regards,
Ernesto.
0 件の賞賛
返信

3,503件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
You probably only should have your own C files in your project to create the library, well it depends on what the library is for.
For a general purpose lib, I would not put the ansi*.lib, start*.c, datapage.c inside of it.

PS: What for a library do you create anyway?
0 件の賞賛
返信

3,503件の閲覧回数
etolocka
Contributor I
I want to create a library with general functions for several text LCDs.

Another question: What about the header file? Do I need to include it in one of the ".c" files? (e.g. the first one) using the "include" directive?

Regards,
Ernesto.
0 件の賞賛
返信