MC9S12XEP100 data jumping when the software is running

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12XEP100 data jumping when the software is running

985 Views
金翅大鹏鸟
Contributor II

I run the software on the platform MC9S12XEP100MAL. But when I monitor the data with INCA(a tool),I can see that the data is jumping with no regularity,for example , the data now is 500,it can change to 5000 in very short fulture time.But the software is running without reset,because the counter that I set in the while(1) is counting all the time.The application software is generated by Simulink.

Labels (1)
0 Kudos
Reply
1 Reply

923 Views
BlackNight
NXP Employee
NXP Employee

I don't know INCA, but I assume it reads the data over a serial line or similar. In that case your problem is that INCA tool which is not able to meet the realtime requirements to read the data a true periodic intervals. I suggest you contact the vendor of that tool.

I hope this helps,

Erich

0 Kudos
Reply