Lockup with CW3.1 for HS08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lockup with CW3.1 for HS08

Jump to solution
2,551 Views
johnm
Contributor I
I am using a standard registered version of CW 3.1 for HCS08.
When using it the program will lock up completely, usually after a few minutes.
This happens even when just browsing code.  It happens pretty much every time
I use CW.  I am running Win XP SP1, but could possibly get SP2 installed if it may help.
Regards
John
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,646 Views
J2MEJediMaster
Specialist I
Are you using a firewall? That's been known to cause some problems, particularly if you're using a floating license. Also, go to the bottom of this Web page, and try entering the search string "Codewarrior hang" (no quotes), and examine some of the threads on this subject.

---Tom

Message Edited by J2MEJediMaster on 2006-09-27 09:36 AM

View solution in original post

0 Kudos
Reply
2 Replies
1,647 Views
J2MEJediMaster
Specialist I
Are you using a firewall? That's been known to cause some problems, particularly if you're using a floating license. Also, go to the bottom of this Web page, and try entering the search string "Codewarrior hang" (no quotes), and examine some of the threads on this subject.

---Tom

Message Edited by J2MEJediMaster on 2006-09-27 09:36 AM

0 Kudos
Reply
1,646 Views
Alban
Senior Contributor II
I had similar trouble on CW 4.5 for S12 which disappeared when I re-installed Symantec Anti-Virus.
Alban.