Loading code into S12X problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Loading code into S12X problems

ソリューションへジャンプ
4,845件の閲覧回数
ThomasG
Contributor I
Hello,
 
I am working with a MC9S12XDT256 part with Codewarrior for HC12 Professional Edition and am having trouble after I load the code into flash.
 
The loading of the S19 file seems to go ok but once the program starts running, it stops and says an ILLEGAL_BP error occurred.  This seems to be occuring right away in the startup code (before I get to main).
 
I then looked at the hardware schematics and noticed MODB and MODA are not tied to ground or VDD.  The hardware designer left one of the pins open while using another pin as a GPIO pin to an external hardware chip.
 
My question is there anything else I should be making sure I setup as part of the startup process or is it not working because the MODB and MODA pins are not connected properly.  If this is the case, am I out of luck or is there a possible workaround?
 
Thank you,
 
Thomas
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,745件の閲覧回数
CrasyCat
Specialist III
Hello
 
  ILLEGAL_BP just notifies you that the application reaches an invalid code position.
  First thing I would suspect here is that an un-initialized interrupt arises somewhere in your code.
 
  But there might be other reason for that behavior.
  From here you have two solutions:
     1- Try to debug from the application entry point to figure out what is happening before main
          To tell the debugger it should stop at the application entry point:
            - Start the debugger the usual way
            - Select File -> "Configuration"
            - Switch to the "Load" tab.
            - Uncheck the box "Run after successful load"
            - Close the debugger and restart it.
         Application should now stop directly at application entry point. You can step from here and
         check what is happening.
    2- You can submit a service request  for that.
        To log the issue please go to following URL: 
            http://www.freescale.com/TechSupport
        and click on "Submit a service request"
        Make sure to attached a reproducible project to the request. You can collect information
        needed for the service request using the Pack and Go wizard.
        Just select Help -> "Pack and Go" and follow the instruction on the screen.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,745件の閲覧回数
ThomasG
Contributor I
Thank you for the replies.
 
I may try to somehow ground the MODA and MODB signals lines on power-up and see if anything changes.
0 件の賞賛
返信
3,745件の閲覧回数
Alban
Senior Contributor II
Hello Thomas,
 
It is imperative that MODx pins are at appropriate level when a reset occurs.
There is no workaround as the hardware will decide which mode (External Bus, Single Chip, BDM...) the MCU should run in when reset is happening. At that point no software is executed yet.
 
Sorry...
 
Alban.
3,745件の閲覧回数
CrasyCat
Specialist III
Hello
 
  ILLEGAL_BP just notifies you that the application reaches an invalid code position.
  First thing I would suspect here is that an un-initialized interrupt arises somewhere in your code.
 
  But there might be other reason for that behavior.
  From here you have two solutions:
     1- Try to debug from the application entry point to figure out what is happening before main
          To tell the debugger it should stop at the application entry point:
            - Start the debugger the usual way
            - Select File -> "Configuration"
            - Switch to the "Load" tab.
            - Uncheck the box "Run after successful load"
            - Close the debugger and restart it.
         Application should now stop directly at application entry point. You can step from here and
         check what is happening.
    2- You can submit a service request  for that.
        To log the issue please go to following URL: 
            http://www.freescale.com/TechSupport
        and click on "Submit a service request"
        Make sure to attached a reproducible project to the request. You can collect information
        needed for the service request using the Pack and Go wizard.
        Just select Help -> "Pack and Go" and follow the instruction on the screen.
 
CrasyCat
0 件の賞賛
返信