Shortcuts for set bookmark, previous bookmark, next bookmark?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shortcuts for set bookmark, previous bookmark, next bookmark?

Jump to solution
1,368 Views
BasePointer
Contributor II
Hi,
 
How can I navigate in code shortly?
What are the keyboard shortcuts for set bookmark, previous bookmark, next bookmark?
 
Codewarrior v5.1 for HCS08.
 
Thank you,
BP.
Labels (1)
Tags (1)
0 Kudos
1 Solution
508 Views
CrasyCat
Specialist III
Hello
 
You can look at all shortcuts defined in the IDE in the "Customize IDE Commands" dialog.
 
You can open this dialog through "Edit" -> "Commands and Key Bindings".
In the Command Tab, expand the "Editor Commands" and scroll down a bit.
You will notice that
    Shortcut to Add a Bookmark is CTRL+F2
    Shortcut to Go to next bookmark is F2
    Shortcut to Go to previous bookmark is SHIFT+F2
 
Note that you can use that dialog to define your own shortcuts if you wish.
This only works if you select a key combination, which is not used for something else.
 
I hope it helps. 
 
CrasyCat

View solution in original post

0 Kudos
2 Replies
509 Views
CrasyCat
Specialist III
Hello
 
You can look at all shortcuts defined in the IDE in the "Customize IDE Commands" dialog.
 
You can open this dialog through "Edit" -> "Commands and Key Bindings".
In the Command Tab, expand the "Editor Commands" and scroll down a bit.
You will notice that
    Shortcut to Add a Bookmark is CTRL+F2
    Shortcut to Go to next bookmark is F2
    Shortcut to Go to previous bookmark is SHIFT+F2
 
Note that you can use that dialog to define your own shortcuts if you wish.
This only works if you select a key combination, which is not used for something else.
 
I hope it helps. 
 
CrasyCat
0 Kudos
508 Views
BasePointer
Contributor II
Thank you!
0 Kudos