Load the program in batch for S08

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Load the program in batch for S08

1,530件の閲覧回数
lelam
Contributor II

Hi team!

I am using MCU MC9S08PT for our product
My problem now is that when the mass production (Average 500,000pcs / year), now workers have to load the program one by one (Using CodeWarrior and Multilink Universal FX), it takes too much time and does not reach production capacity.
Is there a better way for us? For example, program loader 1 for many products
Note: We change the design constantly for different products so do not pre-load firmware from the supplier

Thank you.

0 件の賞賛
返信
1 返信

1,447件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Le,

 

An option would be to use Cyclone-FX for production programming. Programming may be launched by a single button press without a host PC or automatically from a PC via the automated control SDK.

 

Also, please check the Flash File to Target feature of Codewarrior. You can find more information in

CodeWarrior Development Studio Common Features Guide.

 

I hope this helps.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信