Hello Le,
An option would be to use Cyclone-FX for production programming. Programming may be launched by a single button press without a host PC or automatically from a PC via the automated control SDK.
Also, please check the Flash File to Target feature of Codewarrior. You can find more information in
CodeWarrior Development Studio Common Features Guide.
I hope this helps.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------