Linker Script In Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linker Script In Bootloader

1,840件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    How to Edit Linker Scrip in a Bootloader?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,663件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

in addition, I recommend you refer document:

Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+

"3.3.3. Bootloader Linker File Revision" is regarding how to revise bootloader linker file

"3.3.8. User application code" includes how to revise user app linker file.

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,664件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Vignesh

By default, user just needs to ensure that the code and global data are placed in flash pages which are separated with application. And the jump address for Reset Vector should be set to the start address of bootloader. 

If there is any further question, please reply, and please also supply the part number of your target MCU. Thanks! 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 件の賞賛
返信