Link ram and flash routines

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Link ram and flash routines

785 次查看
albertomainoni
Contributor I

Hi,

I need to run about 70KB of code faster. I think that running it in ram could increase the speed enough.

The software size is too big to run all  in ram so I need to use some code in flash and other in ram.

Some routines in ram have to call some routines in flash and vice versa.

Please is there a sample code that can load an executable library in ram at than calling routines (with codewarrior, micro k60)?

Thank you

Alberto

 

标签 (1)
标记 (4)
0 项奖励
回复
0 回复数