Link ram and flash routines

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Link ram and flash routines

778件の閲覧回数
albertomainoni
Contributor I

Hi,

I need to run about 70KB of code faster. I think that running it in ram could increase the speed enough.

The software size is too big to run all  in ram so I need to use some code in flash and other in ram.

Some routines in ram have to call some routines in flash and vice versa.

Please is there a sample code that can load an executable library in ram at than calling routines (with codewarrior, micro k60)?

Thank you

Alberto

 

ラベル(1)
タグ(4)
0 件の賞賛
返信
0 返答(返信)