Launching to Debugger Engine hangs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Launching to Debugger Engine hangs

3,425件の閲覧回数
rowancarter
Contributor I

I have created a FLASH Programmer task, yet when I run it the following is the output I get.

 

5286_5286.pngScreenshot.png

 

I am using Linux version of CodeWarrior

Installed Products:

- CodeWarrior for Power Architecture

     Version: 10.3

     Build Id:130315

 

I had this running on a Windows Codewarrior v10.1.1 but am now stuck at this point having migrated to Linux.

 

Any help gratefully received.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,058件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

Can you please provide the board name and the Linux distribution?

Also, can you please verify if you have any DE or ccs hanged processes?

Thank you,

Marius

0 件の賞賛
返信

3,058件の閲覧回数
rowancarter
Contributor I

Hi, the target is our own hardware with a P2020 on it. We have

successfully used the CW PA 10.1.1 (WinXP) with this hardware, via

USB-TAP.

Linux is CentOS 5.9

cwde process is sleeping, no ccs processes

Thanks

Rowan

0 件の賞賛
返信

3,058件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi, 32 or 64bits?

Thanks,

Marius

0 件の賞賛
返信

3,058件の閲覧回数
rowancarter
Contributor I

Sorry,

64 bit

Rowan

0 件の賞賛
返信

3,058件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

There is any chance to upgrade to CentOS 6.3? Officially, we don't support CentOS 5.9. According with the information from README.txt file we support only next distributions:

   32 bit

      2.1 RedHat Enterprise Linux 5.4

      2.2 Ubuntu 8.04

      2.3 Ubuntu 9.10

      2.4 Fedora Core 11

      2.5 Suse 11 Server

      2.6 RedHat Enterprise Linux 4

      2.7 Ubuntu 10.04

   64 bit

      2.8 RedHat Enterprise Linux Server 5.4

      2.9 RedHat Enterprise Linux 4

      2.10 Fedora Release 11

      2.11 Suse Linux Enterprise Server 11

      2.12 Ubuntu 10.04

      2.13 Ubuntu 11.04

      2.14 CentOS 6.3

      2.15 libexpat system library

Regards,

Marius

0 件の賞賛
返信

3,058件の閲覧回数
rowancarter
Contributor I

Hi,

sadly our dev environment needs to be the old CentOS version - I am

looking at possibly providing an upgrade, also requested a Windows

download that may get us going.

Thanks

Rowan

0 件の賞賛
返信