Keil uLink 2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,406件の閲覧回数
juliancox
Contributor V

Does anyone know if the KEIL ULINK 2 probe can be used with CodeWarrior or (more useful to me) the USBDM programming utility? I know that the pod will support Single Wire Debug.

タグ(2)
0 件の賞賛
返信
1 解決策
2,223件の閲覧回数
juliancox
Contributor V

This is an option for ARM (which is why I have a ULINK 2) but Keil does not support S08 devices.

元の投稿で解決策を見る

2 返答(返信)
2,223件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Julian,

CodeWarrior and USBDM doesn't support KEIL ULINK 2 .

If you use ULINK2, please consider KEIL MDK.

Please
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,224件の閲覧回数
juliancox
Contributor V

This is an option for ARM (which is why I have a ULINK 2) but Keil does not support S08 devices.