Keil uLink 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keil uLink 2

Jump to solution
2,397 Views
juliancox
Contributor V

Does anyone know if the KEIL ULINK 2 probe can be used with CodeWarrior or (more useful to me) the USBDM programming utility? I know that the pod will support Single Wire Debug.

Tags (2)
0 Kudos
Reply
1 Solution
2,214 Views
juliancox
Contributor V

This is an option for ARM (which is why I have a ULINK 2) but Keil does not support S08 devices.

View solution in original post

2 Replies
2,214 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Julian,

CodeWarrior and USBDM doesn't support KEIL ULINK 2 .

If you use ULINK2, please consider KEIL MDK.

Please
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,215 Views
juliancox
Contributor V

This is an option for ARM (which is why I have a ULINK 2) but Keil does not support S08 devices.