KSDK_PATH error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK_PATH error

2,292件の閲覧回数
Fan_xy
Contributor III


Hello

 

My kds 1.1.1 and KDS 2.0.0 now all error when creat KSDK project .

Before I have create KSDK project work well and run the KSDK demo code work well too, while now , it error like this

 

I'm sure I have config the varialbe on the computer properies refer to the user guide.

 

17555_17555.png222222222.png

 

please tell me how to solve it !

 

Than you a lot !

 

Linda

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,919件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Linda,

what is the content of your KSDK_PATH variable?

Erich

0 件の賞賛
返信

1,919件の閲覧回数
Fan_xy
Contributor III

Hi Erich,

I think there is an error in the DOC "C:\Freescale\KSDK_1.0.0\doc\Kinetis SDK k64 User's Guide"

s.png

Best Regards

Linda

0 件の賞賛
返信

1,919件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Linda,

yes, this is obviously an error :-( I have passed this to the engineering team so they can review/fix it.

The variable needs to point to your Kinetis SDK folder, e.g.

C:\Freescale\KSDK_1.0.0

Erich

0 件の賞賛
返信