KL16Z256M4 Codewarrior setup "vague" error: Which name?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL16Z256M4 Codewarrior setup "vague" error: Which name?

跳至解决方案
1,442 次查看
djmp
Contributor I

With Multylink programmer connected to Freescale MCU KL16Z256M4, an error is reported back  in Hardware Connection>>Advanced Programming Options:  "Device name could not be determined".

Which name? Is just the name it's missing? Never had seen this error!

Setup settings and MCU are ok since it work correctly on different machines. Any clue for this "vague" error.

Thanks.

David Palma

标签 (1)
0 项奖励
回复
1 解答
1,366 次查看
trytohelp
NXP Employee
NXP Employee

Hi David,

Do you use CW for MCU V10.6 ?

    Else what is the tool version ?

CW for MCU v10.6.4 is the last version.

A patch V10.6.5 can be installed too.

The P&E interfaces Mulitlink are supported by this configuration.

Now it could be important to know exactly the name of interface and rev.

There are several Multilink interfaces.

To test it I recommend to create a sample project (project Wizard) for your hardware configuration.

With this example, you should be able to load the example on board without problem.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,367 次查看
trytohelp
NXP Employee
NXP Employee

Hi David,

Do you use CW for MCU V10.6 ?

    Else what is the tool version ?

CW for MCU v10.6.4 is the last version.

A patch V10.6.5 can be installed too.

The P&E interfaces Mulitlink are supported by this configuration.

Now it could be important to know exactly the name of interface and rev.

There are several Multilink interfaces.

To test it I recommend to create a sample project (project Wizard) for your hardware configuration.

With this example, you should be able to load the example on board without problem.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复