JL8 Programming Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JL8 Programming Error

ソリューションへジャンプ
2,546件の閲覧回数
mlogix
Contributor I
Hi,
We are getting an error while programming the JL8 controller. It reads like this - "Communication error between the instrument and the target system. Error occurred after successfully entering the monitor mode. Verify communication parameters and retry!"

Is there anybody to help me out?
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,803件の閲覧回数
bespenschied
Contributor III
How are you interfacing to your target? I use an in-house designed MON08 Interface and it generates the required Vtst, MOD0, MOD1 and DIV4 signals. If the Vtst is on the IRQ pin(1), PTB1 (MOD0) pin(20) is tied to Vdd with a 10K Resistor, PTB2 (MOD1) pin (18) is tied to Ground with a 10K resistor, and PTB3 (DIV4) Pin(17) is tied either high or low with a 10K resistor depending on what your clock is. If you use a 9.8304 MHz clock source and PTB3 is high your Baud rate will be 9600 Baud. If PTB3 is Low your Baud Rate will be 19200. If you use a 4.9125MHz and PTB3 is LOW you get a 9600 Baud rate.

Double check your voltage levels on the required MON08 pins. Make sure your Vtst is the correct voltage also. Vtst according to the datasheet should be between 7.5V and 8.5V with a 5V Vdd supply.

I hope this helps.

Brian

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,804件の閲覧回数
bespenschied
Contributor III
How are you interfacing to your target? I use an in-house designed MON08 Interface and it generates the required Vtst, MOD0, MOD1 and DIV4 signals. If the Vtst is on the IRQ pin(1), PTB1 (MOD0) pin(20) is tied to Vdd with a 10K Resistor, PTB2 (MOD1) pin (18) is tied to Ground with a 10K resistor, and PTB3 (DIV4) Pin(17) is tied either high or low with a 10K resistor depending on what your clock is. If you use a 9.8304 MHz clock source and PTB3 is high your Baud rate will be 9600 Baud. If PTB3 is Low your Baud Rate will be 19200. If you use a 4.9125MHz and PTB3 is LOW you get a 9600 Baud rate.

Double check your voltage levels on the required MON08 pins. Make sure your Vtst is the correct voltage also. Vtst according to the datasheet should be between 7.5V and 8.5V with a 5V Vdd supply.

I hope this helps.

Brian
0 件の賞賛
返信