Is there a stdargs.h header file for CW 10.2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a stdargs.h header file for CW 10.2?

Jump to solution
1,185 Views
samsaprunoff
Contributor V

Good day all,

I was curious if there is a "stdargs.h" header file for CW 10.2?  I ask, as I have some legacy could that I would like to port and it uses stdarg.h within some of its routines.  I could go through it and re-write it, but was hoping that there was a stdargs.h that I could use.

 

Thanks in advance!

Cheers,

Sam

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,082 Views
DerekLau
Contributor IV

There are stdarg.h (not stdargs.h) files under the subfolders of \Freescale\CW MCU v10.2\MCU.

View solution in original post

0 Kudos
Reply
2 Replies
1,083 Views
DerekLau
Contributor IV

There are stdarg.h (not stdargs.h) files under the subfolders of \Freescale\CW MCU v10.2\MCU.

0 Kudos
Reply
1,082 Views
samsaprunoff
Contributor V

Good day Derek,

Thanks for your response!  Indeed, I made a mistake in the header file name for some reason I added the "plural" version :smileyhappy:

Cheers,


Sam

0 Kudos
Reply