Integration Library "Automotive Math and Motor Control Library Set for KEAx devices"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Integration Library "Automotive Math and Motor Control Library Set for KEAx devices"

ソリューションへジャンプ
1,746件の閲覧回数
kuanyuenliao
Contributor II

Hello,

  I am building a motor control project by CodeWarrior ver. 10.6,  follow the guide "Automotive Math and Motor Control Library Set for KEAx devices User's Guide", and work on "3.10 Library Integration into a Freescale CodeWarrior Eclipse IDE"‧

  

  Then I have the problem:

  1) The environment is different between the guide figure and CW IDE, so I cannot sure if I have done the library linking or not.

  2) After built, I got the error message:

DescriptionResourcePathLocationType
cannot find -lD:FreescaleAMMCLIBKEAx_AMMCLIB_v1.1.2libcw10xKEAx_AMMCLIB.UC.aaaaaC/C++ Problem

  Besides the slash,it's the right address.

  thanks!

ラベル(1)
1 解決策
1,605件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello KuanYuen

Please open the Project Properties, remove your old setting for ‘Libraries’ in ‘Paths and Symbols’, add the library instead in the <ARM Ltd  Windows GCC C liner -> Miscellaneous -> other objects>, please see the screenshot in below:

ammclib.png

Does it work?

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,606件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello KuanYuen

Please open the Project Properties, remove your old setting for ‘Libraries’ in ‘Paths and Symbols’, add the library instead in the <ARM Ltd  Windows GCC C liner -> Miscellaneous -> other objects>, please see the screenshot in below:

ammclib.png

Does it work?

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------