Installation Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,148件の閲覧回数
foo223
Contributor I

I'm trying to install Codewarrior HCS12(X) v4.7 and it seems to make it all the way to the end, then says, "Rolling Back Action" for no apparent reason.  Then it simply says that the process was interrupted without supplying any other information.

 

Any help would be greatly appreciated.

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,604件の閲覧回数
foo222
Contributor II

problem solved by deselecting emulator installation on install.  not exactly sure why that worked, but thanks for everyone's help.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,605件の閲覧回数
kef
Specialist I

64bits windows? If yes, then check out this thread

 https://community.freescale.com/thread/57404

0 件の賞賛
返信
2,605件の閲覧回数
foo222
Contributor II

Thanks for your quick reply, but unfortunalty it`s not a 64 bit PC.  I'm using XP.

0 件の賞賛
返信
2,605件の閲覧回数
CrasyCat
Specialist III

Hello

 

Make sure you disconnect all USB devices from your computer before starting installation.

 

Issue may arise if you have a debugging cable from any provider hooked up to one of your USB port when attempting to install.

 

CrasyCat

0 件の賞賛
返信
2,605件の閲覧回数
foo222
Contributor II

problem solved by deselecting emulator installation on install.  not exactly sure why that worked, but thanks for everyone's help.

0 件の賞賛
返信