problem connecting to the board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

problem connecting to the board

跳至解决方案
1,808 次查看
Yuping
Contributor I

Hi All,

 

I have a TSSEVB from Freescale.

I downloaded CodeWarrior v10 for my x64 system and tried to debug one of the microprocessors on the TSSEVB from my PC.

I tried both the 9S08LG32 microprocessor and the 9S08JM60 COMM microcontroller. Neither of them worked. 

 

When I was setting up the debug configuration, I chose P&E HCS08 Multilink\Cyclone Pro for connection, and chose USB HCS08/HCS12/CFV1 Multilink-USB Port as interface. But when I click refresh, there's no available USB port.

 

I had this problem when I was using CodeWarrior 6.3. The driver for the COMM microcontroller couldn't be installed either.

 

Could anyone help with this?

 

Thanks!

 

Yuping

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,418 次查看
J2MEJediMaster
Specialist I

There are some issues with CodeWarrior interoperating with USB on a 64-bit Windows 7 system. You might want to look at the last few pages of this forum thread for some work-arounds.

 

---Tom

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,419 次查看
J2MEJediMaster
Specialist I

There are some issues with CodeWarrior interoperating with USB on a 64-bit Windows 7 system. You might want to look at the last few pages of this forum thread for some work-arounds.

 

---Tom

0 项奖励
回复