Installation Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installation Problem

Jump to solution
3,135 Views
foo223
Contributor I

I'm trying to install Codewarrior HCS12(X) v4.7 and it seems to make it all the way to the end, then says, "Rolling Back Action" for no apparent reason.  Then it simply says that the process was interrupted without supplying any other information.

 

Any help would be greatly appreciated.

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,591 Views
foo222
Contributor II

problem solved by deselecting emulator installation on install.  not exactly sure why that worked, but thanks for everyone's help.

View solution in original post

0 Kudos
Reply
4 Replies
2,592 Views
kef
Specialist I

64bits windows? If yes, then check out this thread

 https://community.freescale.com/thread/57404

0 Kudos
Reply
2,592 Views
foo222
Contributor II

Thanks for your quick reply, but unfortunalty it`s not a 64 bit PC.  I'm using XP.

0 Kudos
Reply
2,592 Views
CrasyCat
Specialist III

Hello

 

Make sure you disconnect all USB devices from your computer before starting installation.

 

Issue may arise if you have a debugging cable from any provider hooked up to one of your USB port when attempting to install.

 

CrasyCat

0 Kudos
Reply
2,592 Views
foo222
Contributor II

problem solved by deselecting emulator installation on install.  not exactly sure why that worked, but thanks for everyone's help.

0 Kudos
Reply