ISScript problem during CW4.7 installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISScript problem during CW4.7 installation

ソリューションへジャンプ
3,716件の閲覧回数
paul_kdg
Contributor I
I try to install the codewarrior 4.7 on my PC (running XP), but I get following message during the installation process:
 
"The InstallScript engine is missing from this machine.  If available, please run ISScript.msi, (etc...)"
 
I tried the same on a different PC, and I even tried to re-install the older version (4.6) which I still had on CD.  It all turned out to the same problem.
 
What can I do?
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,202件の閲覧回数
paul_kdg
Contributor I
Problem solved.
The root cause was that on my PC, there was already an installation programme (called "InstallScriptMSIEngine" ) present.  This was apparently conflicting with the installation procedure of the codewarrior.  I simply removed the InstallScriptMSIEngine software.  After this action, CW installation succeeded.
 


Message Edited by paul@kdg on 2008-12-05 11:24 AM

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,203件の閲覧回数
paul_kdg
Contributor I
Problem solved.
The root cause was that on my PC, there was already an installation programme (called "InstallScriptMSIEngine" ) present.  This was apparently conflicting with the installation procedure of the codewarrior.  I simply removed the InstallScriptMSIEngine software.  After this action, CW installation succeeded.
 


Message Edited by paul@kdg on 2008-12-05 11:24 AM
0 件の賞賛
返信
2,202件の閲覧回数
J2MEJediMaster
Specialist I
If you can, try to download the free Special Edition of CodeWarrior for HSC12(X) from this page. If that works, then the CD might be bad. If that download fails to install, it might be that something has corrupted the standard installer software on the system. Also, are you running any virus-protection software that might be interpreting the installation as a virus trying to infect the machine?

---Tom
0 件の賞賛
返信