ISScript problem during CW4.7 installation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ISScript problem during CW4.7 installation

跳至解决方案
3,781 次查看
paul_kdg
Contributor I
I try to install the codewarrior 4.7 on my PC (running XP), but I get following message during the installation process:
 
"The InstallScript engine is missing from this machine.  If available, please run ISScript.msi, (etc...)"
 
I tried the same on a different PC, and I even tried to re-install the older version (4.6) which I still had on CD.  It all turned out to the same problem.
 
What can I do?
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,267 次查看
paul_kdg
Contributor I
Problem solved.
The root cause was that on my PC, there was already an installation programme (called "InstallScriptMSIEngine" ) present.  This was apparently conflicting with the installation procedure of the codewarrior.  I simply removed the InstallScriptMSIEngine software.  After this action, CW installation succeeded.
 


Message Edited by paul@kdg on 2008-12-05 11:24 AM

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,268 次查看
paul_kdg
Contributor I
Problem solved.
The root cause was that on my PC, there was already an installation programme (called "InstallScriptMSIEngine" ) present.  This was apparently conflicting with the installation procedure of the codewarrior.  I simply removed the InstallScriptMSIEngine software.  After this action, CW installation succeeded.
 


Message Edited by paul@kdg on 2008-12-05 11:24 AM
0 项奖励
回复
2,267 次查看
J2MEJediMaster
Specialist I
If you can, try to download the free Special Edition of CodeWarrior for HSC12(X) from this page. If that works, then the CD might be bad. If that download fails to install, it might be that something has corrupted the standard installer software on the system. Also, are you running any virus-protection software that might be interpreting the installation as a virus trying to infect the machine?

---Tom
0 项奖励
回复