IO pin status during debug.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IO pin status during debug.

ソリューションへジャンプ
1,992件の閲覧回数
juliancox
Contributor V

Is it possible to monitor the status of I/O pins in CodeWarrior during a debug session using Multilink? I would like to see the configuration and pin output value (logical, of course) as I single-step through the code. I can measure the actual voltage, but this does not match the value written to the pin register. 

タグ(3)
0 件の賞賛
返信
1 解決策
1,843件の閲覧回数
juliancox
Contributor V

Thanks, it answers my question. I am migrating from KEIL IDE (LPC9XX) and they display a peripheral as a graphic in which I can set/clear any bit in any register by clicking on the appropriate box. I guess I was looking for something similar. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,844件の閲覧回数
juliancox
Contributor V

Thanks, it answers my question. I am migrating from KEIL IDE (LPC9XX) and they display a peripheral as a graphic in which I can set/clear any bit in any register by clicking on the appropriate box. I guess I was looking for something similar. 

0 件の賞賛
返信
1,843件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian,

Yes, you can check the related register on Register view on CW:

pastedImage_1.png

Please enable the "Refresh While Running" , then register can  update in running time .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信