typedef unsigned char time_Sound; #define timeSound1 0x04 ... timeSound |= timeSound1;
If this is a copy from your sound.c file, the problem is time_TimeSTR is not the typedef name you declared in the header, it is time_SoundSTR. Also, the extern is defined as _time_Sound, time with a lower case t instead of the upper case you have used here.
UtopiaTim wrote:#include "sound.h"time_TimeSTR _Time_Sound;
In sound.h, I have specified that it should be on the 1st page, have I missed anything in that regard?
Thanks,
Tim
#ifndef TIME_SOUND_HEADER  // These 2 lines are an include guard, to make sure this file#define TIME_SOUND_HEADER  // is only included once in any one source filetypedef union { byte Byte; struct {   byte NC1        :1;   byte NC2        :1;   byte time1Sound :1;   byte time2Sound :1;   byte time3Sound :1;   byte time4Sound :1;   byte time5Sound :1;   byte time6Sound :1; } Bits;} time_SoundSTR;   extern time_SoundSTR _time_Sound;#define time_Sound     _time_Sound.Byte#define NC1            _time_Sound.Bits.NC1#define NC2            _time_Sound.Bits.NC2#define time1Sound     _time_Sound.Bits.time1Sound#define time2Sound     _time_Sound.Bits.time2Sound#define time3Sound     _time_Sound.Bits.time3Sound#define time4Sound     _time_Sound.Bits.time4Sound#define time5Sound     _time_Sound.Bits.time5Sound#define time6Sound     _time_Sound.Bits.time6Sound#endif  // End of the include guardDid you define the variables after include the header file in one C file? Usually that is the C file with the corresponding name, e.g.
/* sound.c */#include "sound.h"time_SoundSTR _time_Sound;