How to get the machine code file from a target board with an un-protected or un-secured Flash MCU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get the machine code file from a target board with an un-protected or un-secured Flash MCU?

649 次查看
kunxu
Contributor II

Hello, I have a target board with a MC9S12XEP100 chip. The flash of the MCU chip is un-protected and un-secured. I want to get the machine code file or assembly file (*.abs, or *.s19). What should I do?

PS: I have succesfully connected the target board using the BDM (P&E USB Multilink Inerface) via the software - hiwave.exe, and see the contents of the Flash memory, as well as the Assemble codes  in the Windows of "Memory" and "Assemble" of the hiwave.exe software, respectively. But I don't know how to save them as a *.abs file or a *.s19 file.  The copy command cannot be used in the Windows "Memory" or "Assemble" of the hiwave.exe software

标签 (1)
0 项奖励
回复
0 回复数