Hello guys,
Is there a way I can generate a half-bridge pwm signals with dead-time using coldfire v1 ?
I'm using the mcf51jm128
I need to generate two complementary pwm signals with a dead-time in between the up and down of each others.
Frequency around 60-100khz would be enough.
It could also be done setting a duty cycle under 50% and being able to delay one pwm from another.
You'll be able to find context schematics attached.
Any help would be great,
Thanks already !