Hi Carlos
We are developping a new device where up to 4 amperometric sensors are
connected to it and can be configured in different ways. The entire
configuration settings, calibration data and signal outputs are handled
by a MK20DN512 MCU. We have recieved the entire code from another
company which is working on the hardware (and according software) part
of the project. Our expertise is the sensor part but we want to
familiarize ourselves with the MCU programming too since the device will
be sold to our customers and we need the expertise in house.
We are using home-built libraries.
Yes, our project requieres MQX.
In the meanwhile I found that MQX was simply missing on my PC and I
installed it. I have been looking through your tutorials to understand
what I should do. In principle, it should be simple: (i.) Create
Libraries with MQX, (ii.) Build Project in Code Warrior and (iii.)
Create flash image file.
So far, as I mentioned in my previous post, I have found out how to to
step 2 and 3 using a freescale tower and some example project. With our
own code I am still struggeling at step 1. I am not able to build the
/Project.cw10gcc/ folder with its corresponding subfolders /debug/ and
/release/. If I manage this, everything else should work. Any
suggestions there? I have tried the MQX Clone Wizard but this is not
giving me the correct compiled folder.
Best regards
Jorge
Am 15.02.2018 um 19:41 schrieb Carlos_Mendoza:
>
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>
Re: How to fix "Invalid project path"?
reply from Carlos_Mendoza
<https://community.nxp.com/people/Carlos_Mendoza?et=watches.email.thread>
in /CodeWarrior for MCU/ - View the full discussion
<https://community.nxp.com/message/987531?commentID=987531&et=watches.email.thread#comment-987531>
>