How to create verification environment for LS1021 ARM processor using TCL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to create verification environment for LS1021 ARM processor using TCL

1,235件の閲覧回数
akkii_133
Contributor I

I have to create verification environment for our project. ARM processor ls1021A connected with code warrior. So how to configure for verification?

ラベル(1)
0 件の賞賛
返信
1 返信

1,145件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ankit Patel,

I assume you mean you are porting CodeWarrior initialization file to execute it on your custom board.

Please refer to the initialization file in C:\Freescale\CW4NET_v2016.01\CW_ARMv7\ARMv7\ARM_Support\Configuration_Files\LS1021A.

Probably you need to modify QSPI(SPI) init, IFC init and DDR init according to your target board.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信