How to create .phy file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to create .phy file

跳至解决方案
4,165 次查看
jensb
Contributor I
On the P&E mirco I read that for downloading a project I needed a *.phy (or convert an *.s19 to *.phy) file. Since I'm Using the codewarrior, it should be possible to directly create a .phy file. But I can't find the info to do so. Does any one has any idea to create such a file?
 
Thx.
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,558 次查看
CrasyCat
Specialist III

Hello

I assume you are using CodeWarrior HC12 V3.1 ot V4.5 . Am I right?

If you create your project using the wizard, there is a file with extension .abs.phy created in the project bin directory.

This is the S record file containing physical addresses.

For the little story, this file is generated by the burner utility when it process the file burner.bbl located in the project prm directory.

Check commands in this file after the comment:
/* physical s-record file */
I hope this helps.

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,559 次查看
CrasyCat
Specialist III

Hello

I assume you are using CodeWarrior HC12 V3.1 ot V4.5 . Am I right?

If you create your project using the wizard, there is a file with extension .abs.phy created in the project bin directory.

This is the S record file containing physical addresses.

For the little story, this file is generated by the burner utility when it process the file burner.bbl located in the project prm directory.

Check commands in this file after the comment:
/* physical s-record file */
I hope this helps.

CrasyCat

0 项奖励
回复
1,558 次查看
jensb
Contributor I

Thx for the help,

The burner.bbl file was not in my project and that was the reason way the .abs file wasn't converted.

Cheers,

jensb

0 项奖励
回复