How to copy a project and rename it.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to copy a project and rename it.

7,513 次查看
GeneGoff
Contributor III

How can you copy a project, then rename it?  If I copy the entire contents of a project into a new folder in Explorer, then import the project into CW, then try to right click on the project in the project pane and try to 'Rename' it, I get a 'refactor exception' error.  I'm running CW for MCU 10.4. 

标签 (1)
标记 (2)
6 回复数

3,457 次查看
Ben
Senior Contributor I

I just copy the project folder, rename it, then import the project to CW workspace.

I found it a simple way, and it works OK

0 项奖励
回复

3,457 次查看
GeneGoff
Contributor III

Thank you.  The new copied project compiles fine, but there are many project settings files, debugger files, and the project name itself in the Project pane which still show the old project name.  If I right click on the project name and click Rename, this was when it gave me the refactor exception error.

0 项奖励
回复

3,457 次查看
Ben
Senior Contributor I

Gene, I don't quite understand you: From my point of view, there are 2 reasons to copy a project and work on the new one:

1) if I want to freeze a project and work on a new revision. In this case, I don't mind that the project and files have the same name.I just rename the folder name.

2) If I want to start a new project, but want to use all teh system profile from an old project. The IDE enable you to start a new project and import the profile from another.

So, if you need a 3rd option, please clarify your needs.

Brgds,

0 项奖励
回复

3,457 次查看
TICS_Fiona
NXP Employee
NXP Employee

3,457 次查看
robertofrechill
Contributor III

Thanks! this help was useful :smileywink:

0 项奖励
回复

3,457 次查看
GeneGoff
Contributor III

Thank you for helping, but when I right click on a project, Copy, then Paste it in the Projects pane, many source files do not get copied as viewed in Windows Explorer.  Consequently when I try to build there are many compile errors.

0 项奖励
回复