How to check CPU usage in CW10.6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check CPU usage in CW10.6?

ソリューションへジャンプ
1,420件の閲覧回数
sourabhpatil
Contributor I

what settings should be done in CW?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,350件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Sourabh,

Strange ...

This should be installed by default.

Attached you will find some manuals contained in the \CW MCU v10.6.4\MCU\Help\PDF folder.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,350件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Sourabh,

CW for MCU V10.6 is supporting several architectures.

Each architecture is using his own build tool chain.

We don't have "generic" answer.

By default all linker can generate a map file which is giving an overview of the memory used by an application.

Depending of the architecture, the linker could provide less or more information.

You will find more details in the manuals at \CW MCU v10.6.4\MCU\Help\PDF folder:

    MCU_Build_Tools_Utilities.pdf for HCs08, RS08 and HCs12Z (search linker or map)

    Targeting_Microcontrollers.pdf for all architectures (search linker or map)

    MCU_"Architecture"_Compiler.pdf you will find some linker, map file info.

Hope this will help

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,350件の閲覧回数
sourabhpatil
Contributor I

Hi Pascal,

Thanks for your reply.

I am not able to find above PDF's in \CW MCU v10.6.4\MCU,

Can you please send me the above PDF's?

Regards,

Sourabh

0 件の賞賛
返信
1,351件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Sourabh,

Strange ...

This should be installed by default.

Attached you will find some manuals contained in the \CW MCU v10.6.4\MCU\Help\PDF folder.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信