How to change the source file location?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the source file location?

1,158 Views
danielchai
Senior Contributor I

Hi,

 

When I create a new source file in a project, it will create a xxx.c under the current folder.

How could I set the CW10.4 so that when I create the source file, it will create it in specific folder?

 

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,070 Views
BlackNight
NXP Employee
NXP Employee

It will use the folder you right click on as the default.

If you want to use a specific folder, either type the path or use the browse folder:

new file.png