How can I view the code size of my project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I view the code size of my project?

1,733件の閲覧回数
danielchampagne
Contributor II

I used to use CW version 6.3.1 in order to compile code for a MC9S08JM60 microcontroller.  Since this version of CW is not supported by Windows 7, I had to start using CW for MCU 10.6.4 (which is Eclipse-based).  I do not mind and I have figured out how to set up and compile my project.  The only thing is that I cannot see the code size for the project.  The older version of CW showed the size of the project (and of each individual file/module).

How can I see the code size using the new tool?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,595件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信

1,595件の閲覧回数
danielchampagne
Contributor II

(The "Cross ARM GNU Print Size" option does not exist under the "Tool

Settings" tab.)

0 件の賞賛
返信

1,595件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Daniel,

if you have CW for MCU 10.6.4 installed with the ARM tools, then it comes with the size utility.

You can use it as described here: https://mcuoneclipse.com/2014/05/04/printing-code-size-information-in-eclipse/ with a 'post build' action.

The thing is that the S08 tools produce the .abs file which is a ELF/Dwarf file, which can be consumed by the size tool.

I hope this helps,

Erich

0 件の賞賛
返信

1,595件の閲覧回数
danielchampagne
Contributor II

Erich,

Thank you for the information. Unfortunately, it does not work for me

as the version of CW for MCU 10.6.4 I am using does not have that

option. It's not an ARM micro but an MC9S08JM60 micro.

Thank you

Daniel

0 件の賞賛
返信