Hotsync to a sleeping HC08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hotsync to a sleeping HC08

Jump to solution
2,699 Views
jckruege
Contributor II

Is it possible to Hotsync to a sleeping HC08 target?

I've tried it and it doesn't seem to work

 

using Codewarrior V6.1 for HC08

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,828 Views
jckruege
Contributor II

I'm trying to connect via BDM to a board running an application, then stop the running applicatioin and inspect memory.  I found my problem; I was using an automated script to program the device, which was also securing the device.  I changed it to not secure the device and .... tada !

 

Thanks for the reply anyway...

 

Jeff

View solution in original post

0 Kudos
Reply
2 Replies
1,828 Views
CrasyCat
Specialist III

Hello

 

What are you trying to do here?

 

Are you trying to connect to a board, where an application is running without any interference to running application?

 

This is possible when you are connected to a HCS08 through a BDM connection.

It is not available when you are connected to a HC08 device through MON08 connection.

 

CrasyCat

0 Kudos
Reply
1,829 Views
jckruege
Contributor II

I'm trying to connect via BDM to a board running an application, then stop the running applicatioin and inspect memory.  I found my problem; I was using an automated script to program the device, which was also securing the device.  I changed it to not secure the device and .... tada !

 

Thanks for the reply anyway...

 

Jeff

0 Kudos
Reply