Hotsync to a sleeping HC08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Hotsync to a sleeping HC08

跳至解决方案
2,684 次查看
jckruege
Contributor II

Is it possible to Hotsync to a sleeping HC08 target?

I've tried it and it doesn't seem to work

 

using Codewarrior V6.1 for HC08

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,813 次查看
jckruege
Contributor II

I'm trying to connect via BDM to a board running an application, then stop the running applicatioin and inspect memory.  I found my problem; I was using an automated script to program the device, which was also securing the device.  I changed it to not secure the device and .... tada !

 

Thanks for the reply anyway...

 

Jeff

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,813 次查看
CrasyCat
Specialist III

Hello

 

What are you trying to do here?

 

Are you trying to connect to a board, where an application is running without any interference to running application?

 

This is possible when you are connected to a HCS08 through a BDM connection.

It is not available when you are connected to a HC08 device through MON08 connection.

 

CrasyCat

0 项奖励
回复
1,814 次查看
jckruege
Contributor II

I'm trying to connect via BDM to a board running an application, then stop the running applicatioin and inspect memory.  I found my problem; I was using an automated script to program the device, which was also securing the device.  I changed it to not secure the device and .... tada !

 

Thanks for the reply anyway...

 

Jeff

0 项奖励
回复