HCS12(X) V4.7 Install problem with error 1722

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS12(X) V4.7 Install problem with error 1722

ソリューションへジャンプ
3,338件の閲覧回数
daveybadlad
Contributor I

Hi, have seen problems on VISTA with this error message but I'm on XPSP2

 

Trying to install CWHCS12X_v4.7.exe gives the following message when progress bar reaches the end:

"Error 1722. There is aproblem with this Windows Installer package. A program run as part of the setupdid not finish as expected"

 

Anyone come across this?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,949件の閲覧回数
daveybadlad
Contributor I

I found the problem!! :smileyhappy:

 

P&E micro (and other codewarrior versions) install windrvr6.sys.  If this driver is loaded already, the installer fails when executing wdreg_gui.exe -inf "C:\Program Files\Freescale\CodeWarrior for HCS12 V4.7\Drivers\windrvr6.inf" install

 

SOLUTION:

Uninstall the windrvr6 driver and remove files so that the installer can re-install them

 

It may also have been possible to disable the P&E micro feature in a custom install??

I'm up and running now anyway! :smileyhappy:

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,950件の閲覧回数
daveybadlad
Contributor I

I found the problem!! :smileyhappy:

 

P&E micro (and other codewarrior versions) install windrvr6.sys.  If this driver is loaded already, the installer fails when executing wdreg_gui.exe -inf "C:\Program Files\Freescale\CodeWarrior for HCS12 V4.7\Drivers\windrvr6.inf" install

 

SOLUTION:

Uninstall the windrvr6 driver and remove files so that the installer can re-install them

 

It may also have been possible to disable the P&E micro feature in a custom install??

I'm up and running now anyway! :smileyhappy:

 

0 件の賞賛
返信
1,949件の閲覧回数
J2MEJediMaster
Specialist I

Are you running the 64-bit version of XP? If so, you may want to look at this thread. Although it's about Vista, the trouble is the same in that it was the 64-bit version that was causing problems for the CodeWarrior installer. That solution might apply here.

 

---Tom

0 件の賞賛
返信