HCS12(X) V4.7 Install problem with error 1722

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS12(X) V4.7 Install problem with error 1722

Jump to solution
3,331 Views
daveybadlad
Contributor I

Hi, have seen problems on VISTA with this error message but I'm on XPSP2

 

Trying to install CWHCS12X_v4.7.exe gives the following message when progress bar reaches the end:

"Error 1722. There is aproblem with this Windows Installer package. A program run as part of the setupdid not finish as expected"

 

Anyone come across this?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,942 Views
daveybadlad
Contributor I

I found the problem!! :smileyhappy:

 

P&E micro (and other codewarrior versions) install windrvr6.sys.  If this driver is loaded already, the installer fails when executing wdreg_gui.exe -inf "C:\Program Files\Freescale\CodeWarrior for HCS12 V4.7\Drivers\windrvr6.inf" install

 

SOLUTION:

Uninstall the windrvr6 driver and remove files so that the installer can re-install them

 

It may also have been possible to disable the P&E micro feature in a custom install??

I'm up and running now anyway! :smileyhappy:

 

View solution in original post

0 Kudos
Reply
2 Replies
1,943 Views
daveybadlad
Contributor I

I found the problem!! :smileyhappy:

 

P&E micro (and other codewarrior versions) install windrvr6.sys.  If this driver is loaded already, the installer fails when executing wdreg_gui.exe -inf "C:\Program Files\Freescale\CodeWarrior for HCS12 V4.7\Drivers\windrvr6.inf" install

 

SOLUTION:

Uninstall the windrvr6 driver and remove files so that the installer can re-install them

 

It may also have been possible to disable the P&E micro feature in a custom install??

I'm up and running now anyway! :smileyhappy:

 

0 Kudos
Reply
1,942 Views
J2MEJediMaster
Specialist I

Are you running the 64-bit version of XP? If so, you may want to look at this thread. Although it's about Vista, the trouble is the same in that it was the 64-bit version that was causing problems for the CodeWarrior installer. That solution might apply here.

 

---Tom

0 Kudos
Reply