HCS08 C: bit field optimization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS08 C: bit field optimization

ソリューションへジャンプ
3,452件の閲覧回数
BasePointer
Contributor II
Hi,
 
I defined LCD segments as bits in a struct.
 
Code:
typedef struct{ unsigned char R0:1; unsigned char R1:1; unsigned char R2:1; unsigned char R3:1; unsigned char R4:1; unsigned char R5:1; unsigned char R6:1; unsigned char R7:1;} TBits;typedef union { unsigned char Val; TBits Bit;} TLcdByte;
#pragma DATA_SEG MY_ZEROPAGE
  TLcdByte LCD_RAM[20];

 
and the definitions:
Code:
#define IND_L1           LCD_RAM[10].Bit.R0#define IND_L2           LCD_RAM[14].Bit.R2#define IND_L3           LCD_RAM[14].Bit.R3#define IND_NL1           LCD_RAM[10].Bit.R2#define IND_NL2           LCD_RAM[14].Bit.R0#define IND_NL3           LCD_RAM[14].Bit.R1#define IND_T1           LCD_RAM[14].Bit.R5#define IND_T2           LCD_RAM[14].Bit.R7#define IND_T3           LCD_RAM[9].Bit.R4#define IND_T4           LCD_RAM[8].Bit.R4
...

 
If I use
Code:
 IND_NL1 = 0; IND_NL2 = 0; IND_NL3 = 0; IND_L1 = 0; IND_L2 = 0; IND_L3 = 0; IND_PP = 0; IND_NP = 0; IND_PQ = 0; IND_NQ = 0;

 

instead of

Code:
IND_NL1 = IND_NL2 = IND_NL3 = IND_L1 = IND_L2 = IND_L3 = IND_PP = IND_NP = IND_PQ = IND_NQ = 0;

it generates more optimal code. Is this normal?

CW v6.1

10x
 


 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,980件の閲覧回数
Lundin
Senior Contributor IV
I believe that the order of evaluation of nested assignments isn't specified by ISO C. So the compiler is free to evaluate the nested assignment in a completely random order, which might give code that isn't possible to optimize.

Another explanation could be that since there is no situation where it is motivated to use nested assignments, perhaps CW doesn't even bother with optimizing them.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,981件の閲覧回数
Lundin
Senior Contributor IV
I believe that the order of evaluation of nested assignments isn't specified by ISO C. So the compiler is free to evaluate the nested assignment in a completely random order, which might give code that isn't possible to optimize.

Another explanation could be that since there is no situation where it is motivated to use nested assignments, perhaps CW doesn't even bother with optimizing them.
0 件の賞賛
返信
1,980件の閲覧回数
BasePointer
Contributor II
Bad compiler.
 
Thanks Lundin.
0 件の賞賛
返信