HCS08 C: What are Profile Analysis and Code Coverage?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS08 C: What are Profile Analysis and Code Coverage?

Jump to solution
2,756 Views
BasePointer
Contributor II
Hi,
 
I nearly finish the project. Now I'm testing and testing... I wonder the test ability of CW. There are two feature of CW. Profile Analysis and Code Coverage. I don't know anything about these analysis technics.
What do they provide me to test my codes?
 
Regards,
BP.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,545 Views
CrasyCat
Specialist III
Hello
 
Neither Profiler nor CodeCoverage can be used on HCS08 hardware board.
 
If you are looking for profiling or Coverage information you may want to look into emulator supporting HCS08 CPUs.
 
CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,546 Views
CrasyCat
Specialist III
Hello
 
Neither Profiler nor CodeCoverage can be used on HCS08 hardware board.
 
If you are looking for profiling or Coverage information you may want to look into emulator supporting HCS08 CPUs.
 
CrasyCat
0 Kudos
Reply