HC08: Error 18 while burning the firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HC08: Error 18 while burning the firmware

跳至解决方案
3,453 次查看
Sany
Contributor III
Hi all, I keep getting "Error 18 during script" when I try to burn my firmware into my HCS08AW60 MCU. I need to repeat the burning process for like 20 to 30 times before it successfully to burn the MCU. I not sure whether this is my own PC problem or my BDM problem. I try this BDM Multilink Interface on other PC before it work well. So I believe it is my pc problem but which part of my pc that cause that Error? The USB port? I noticed that, if I keep the BDM Multilink (USB) connecting my pc while i restart my PC, my PC will hang. Anyone can help? Thank you for spending time reading.

Message Edited by CrasyCat on 2007-04-13 01:59 PM

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,594 次查看
vinze
Contributor I
ok, the problem was the multilink, it wasn't up-to-date. But I don't know why it worked fully on one computeur, and on the other it was able to erase, to read, but not to program...
 
thank you
 
bye.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,595 次查看
vinze
Contributor I
ok, the problem was the multilink, it wasn't up-to-date. But I don't know why it worked fully on one computeur, and on the other it was able to erase, to read, but not to program...
 
thank you
 
bye.
0 项奖励
回复
1,594 次查看
vinze
Contributor I
Hi everybody,
 
I have the same problem than Sany (with MC9S08QE128). Has anyone found the solution since 2007-04-13 ?
 
Thanks.
0 项奖励
回复
1,594 次查看
peg
Senior Contributor IV
Hi vinze,

Given that the description of this error is simply "Error during programming" which is quite unhelpful, I would suggest you post this question direct to P&E themselves here.

0 项奖励
回复