Get Started with MC56F83000EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Get Started with MC56F83000EVK

2,709 次查看
lucasmoraeseng
Contributor II

Hi guys,

I've bought a evaluation board MC56F8300EVK to program its DSC, a PC56F83789. I downloaded CW 11.1, intalled PE drivers and could recognize USB CDC adaptor enabled by OSBDM - JM60. I also configured software DSC56800EX_Quick_Start_r2.7 and imported a example from its folders. I have used to the document https://www.nxp.com/docs/en/user-guide/DSC56800EXQSUG.pdf to get started with the board.

My problem is, after a successful build, I try to run my project and get this error: Error creating session: Invalid target type selection in connection "56F83789_Build_FLASH_SDM_LPM_OSJTAG"

pastedImage_2.png

I've updated the firmware on JM60, but anything I've done, didn't work.

Can anyone help me, please? Is any software missing?

Thank so much for any help.

标签 (1)
2 回复数

2,618 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Lucas,

I have tried to download code with MC56F83000-EVK, it works fine.

I attach the screenshot of software configuration and board configuration.

pastedImage_1.png

I attach the board picture.

BTW, before you download code, you have to pass the compilation and linking stage and  generate the *.elf file which is downloaded to chip.

Hope it can help you

BR

Xiangjun Rong

2,618 次查看
lucasmoraeseng
Contributor II

Thanks so much xiangjun.rong‌.

I missed to full update CW to use with DSC. I downloaded the example again and it works.

Just followed this tutorial: https://www.nxp.com/docs/en/user-guide/INSTALL-CODEWARRIOR-MC56F83XXX.pdf 

Best Regards.

Lucas Moraes

0 项奖励
回复